This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

About delay time of TPS3808G01

Guru 19645 points

Please let me know about delay time of TPS3808G01.

If connect 47kΩ between 5V and CT pin, is this resister influence delay time?

(Schematic is attached below, please see red area)

Best regards,

Satoshi

  • Hi Satoshi,

    The reset delay time is determined by the time it takes for the external capacitor to reach 1.23V. The equations and descriptions in the datasheet assume that only the internal 220nA current source is used to charge the capacitor. By adding a pullup resistor, you are adding an additional current source. As a result, the capacitor will charge faster and the time delay will be shorter.

    Very Respectfully,
    Ryan