I've been using the TPS7A4700 for awhile in various designs and have been pretty happy with it. I have a new application where the TPS7A4700 is disabled in a "low power" mode. During this low power mode, I need to provide reverse current protection to prevent a digital device from back-feeding through the TPS7A4700.
I tried the circuit in the image below but the voltage regulator doesn't seem to work in this configuration. If I jump the diode, it outputs the 3.3V I need but as soon as I remove the jumper shorting the diode, the output goes to 0 (about 0.2V at the output pins, actually). The hope was that, by connecting the sense pin to the load, it would adjust the output for the voltage drop across the diode.
Where did I go wrong? I can always connect the FB pin before the diode but then the output voltage can vary as the current through the diode (and thus Vf) changes.
Thanks!