Dear Experts,
I have a question regarding BQ27x20 usage on host side. When gauge locates on host side, it is possible that gauge will be paired with several different battery packs with different capacity, etc.. It is also possible that battery is charged in external charging dock, meaning that gauge is not connected to battery during charging. How does BQ27x20 perform in a use case where multiple different batteries are used and also charged apart from system?
Both variants of BQ27x20 have several CEDV-profiles. Is profile selected automatically when battery is connected to gauge or is profile always selected by the host?
If BQ27x20 is connected with completely unknown battery with unknown capacity, remaining charge, etc., can you say how long it takes for BQ27x20 to learn the battery?
Rgds,
Juha Pesonen