What is the minimum working voltage parameter value of the ucc28c44 ? I can not find the value in the UCC28C44.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is the minimum working voltage parameter value of the ucc28c44 ? I can not find the value in the UCC28C44.pdf
Hello Ulrich goerke,
I'm using UCC28C44 for dc-dc converter application. The auxiliary winding powers the device after the start-up. But the voltage is not pure dc but half wave rectified. Here how does the controller generates pulses to the MOSFET? And also i have a doubt that if the voltage to power UCC28C44 is pulsating does this allow the start-up circuit to work throughout the application? Your suggestion would greatly support me.
Regards,
deepika
Hello Deepika,
Please refer to the UCC28C44 datasheet Figure 31 on page 24; you'll see that this converter design example also uses an auxiliary winding for the controller bias power. The diode rectifies the winding voltage during the "flyback" interval of the switching cycle. During this time the VDD capacitor Cvdd peak-charges to the winding voltage. This voltage is a one-to-one reflection of the output voltage, so it is about 12V. Cvdd holds this voltage during the primary switching interval and dead times of the switching cycles, so there is no pulsating voltage on VDD. It is a smooth dc level of 12V.
The start-up resistor, in this case, is always "on" the entire time the converter is operating, but the current through this resistor is very low so the power dissipation is small. The start-up VDD current of the UCC28C44 (Istart-up) is less than 100uA, so the start-up resistor Rstart only needs to provide a little more than that to charge up Cvdd. After switching begins, Ivdd increases to several mA, but that power is now provided by the auxiliary winding, even though Rstart is still conducting a few hundred uA.
I hope this answers your questions.
Regard,
Ulrich