Hi,
I am using bq27421-G1A fuel gauge and the battery used is Li-ion battery (3000mAh , 3.8 V).
The Following parameters are written to the Data Memory :
Design Capacity, Design Energy, terminate Voltage, Taper Rate , SOCI Delta , Opconfig .
The SOC interrupt is configured for every 1% change in SOC
The battery voltage is read as 3.8 V . But the SOC read is only 10% .
Why the SOC value is this much low?
Thankyou