Other Parts Discussed in Thread: TPS3820
Hi Tiers.
I can not understanding below.
The watchdog timer can be disabled by disconnecting the WDI pin from the system. If the WDI pin detects that it
is in a high-impedance state the TPS3820/3/4/8 will generate its own WDI pulse to ensure that RESET does not
assert. If this behavior is not desired place a 1kΩ resistor from WDI to ground. This resistor will help ensure that
the TPS3820/3/4/8 detects that WDI is not in a high-impedance state.
If I do not need watchdog, is WDI pin is floated? or 1Kohm Pulled down?