This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Need Support regarding Non Isolated SMPS Design using LM5007

Other Parts Discussed in Thread: LM5007
Dear All,
Here is details of design and problem we are facing with LM5007.
 
We currently using LM5007 Switching IC as Non Isolated Buck Converter with following Specifications.
  • Vin : 12 to 75 VDC
  • Output Voltage : 12 Volt , 4000mA
The reference design is taken from datasheet of LM5007 .
 
We currently facing following queries for reference design.
 
A) With above design we tested it for Vout =12 V,I=250mA for Vin=48 VDC,for this its working fine.
  However when we using it for higher current rating i.e 300 mA or up to 400 mA,we facing Heating of IC which is not desire for our applications.
  We also conducting EMI/EMC test,for that we added FUSIBLE resistor at input,if we ignore this resistor then EMI/EMC Surge test gets failed.
  By keeping resistor we passing Surge test but we getting heating of resistor up to 92°C above 300 mA.So for Surge test we can not ignore this resistor.
 
B) When we using same design with Vin = 24 VDC for Vout = 12 VDC ,I=250 mA,the source current drawing from input is 120mA.So we getting heating of input resistor.
  We also added PTC at Input that also gets open when source current 120 mA.When we removing PTC ,the circuit is working but resistor at input gets Hot.
  For this case No heating of LM5007 were observed. We cannot ignore input resistor for EMI/EMC.
  Please also suggest whether source current is desire or not for this case.
 
C) In LM5007 Specification sheet the current rating is given up to 700 mA , we want to use this device up to 500 mA.
    Please suggest design changes for same.
 
The resistor and PTC used is as below
  • R=47E /5 W
  • PTC 60 Volt ,100mA
I have a attached reference design which we are using currently and reading taken for 48 VDC and 24 VDC.
Power Supply Specifications :
Supply Voltage = 48 VDC , +/-20% i.e 38.4 VDC to 57.6 VDC
Output Voltage = 11.709 VDC at 48 VDC input
Load Current = 250mA Programmable resistor values R1 =3K and R2=820E
Readings of LM 5007 for above specifications
LM5007
Source
Voltage
Source
Current
(mA)
Pin no.8
(VIN)
Pin no.7
(VCC)
Pin no.5
(F/B)
Pin no.1
(SW)
Output Voltage
After Inductor
35 122 27.973 6.981 2.5052 11.672 11.686
38 109 31.7 6.992 2.507 11.665 11.692
39 107 32.86 6.996 2.5072 11.661 11.695
42 98 36.38 7.007 2.5086 11.652 11.701
45 91 39.66 7.017 2.5096 11.644 11.705
48 86 43 7.027 2.5105 11.637 11.709
52 79 47.41 7.039 2.5114 11.629 11.715
55 75 50.61 7.049 2.5121 11.625 11.718
57 74 52.79 7.054 2.5123 11.623 11.719
58 73 53.74 7.057 2.5125 11.622 11.72
60 71 55.88 7.062 2.5129 11.619 11.724
For 24 Vdc input by removing 47 ohm and PTC
24 117 23.25 6.966 2.503 11.675 11.676