This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS62237 - the description VOUT ≤ VIN –1 V on the datasheet P6

Hi all

Would you mind if we ask TPS62237?

There is the description VOUT ≤ VIN –1 V on the datasheet P6.
Our cutomer's condition is as follows;

-Vin=3.6V to 4.2V
-Vout=3.3V
-Iout=0.2A

In this case, we can simulate using Webench.
Does it require 1V difference between Vin and Vout?Or in case of Min Vin(2.05V), does it require 1V difference?

Kind regards,

Hirotaka Matsumoto