This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

High efficiency -48V to +48V isolated dc-dc converter

Other Parts Discussed in Thread: UCC28089, LM5045, LM5046

Looking to develop a converter with >95% eff that has an input range of -36V to -57V and output of the same but positive voltage. So no need for feedback control.

Power 1kW or tandem 500W.