Dear Friends,
I am developing full bridge LLC resonance converter using frequency responce Analysis.
switching frequency should be between 100KHz and 150 kHz in order to maintain ZVS.
Input Voltage range : 380V to 420 V
Output voltage range: 390V to 410Volts
Load range: 20Watts to 5kWatts
Converter should operate in both directions.
Phase shift operation is not required for my case.
Can somebody tell me which controller from TI is suitable for this operation?Please mention complete model.
Right now I am using TMS320F28035 controller card for my Phase shift full bridge topology..Also tell me if its possible to use this for my case as well?
Appreciate your suggestions and help in this matter.