Ho to everyone, what is the right frequency in buck converter for gsm module? A datasheet of one of this recommands a Fsw>750KHz. Is there a requirement for GSM ? Can I use a lower Fsw if I don't have problem of size?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Ho to everyone, what is the right frequency in buck converter for gsm module? A datasheet of one of this recommands a Fsw>750KHz. Is there a requirement for GSM ? Can I use a lower Fsw if I don't have problem of size?
Hi Chris, thank you for your cooperation.
I have need to realize a dc/dc converter to supply a GSM module. I have an input voltage of 4,5 to 24Vdc; I have thought to get an output voltage of 3,8V and 3Apk max (average 500mA).
I have seen the LMR14030 which can run up to 2MHz, but I have found the TPS54xxx family which are more cheap, but they work only up to 400kHz. My doubts are if GSM module needs a minimum Fsw to avoid troubles in the trasmission bandwith.
Thanks
Regards
Simone