Hello,
I have a couple questions regarding the behavior of the BQ24650 under certain circumstances:
1.) Given a Vin = 18V and a Tj in the range of 25 to 100 deg Celcius, What is the maximum power the internal MOSFET driver can withstand?
2.) If Vin is present and MPPT set is >1.2V, if the battery becomes disconnected, what voltage should show on the output?
3.) If Vin is present and MPPT set is equal to 0V, if the battery becomes disconnected, what voltage should show on the output?
I appreciate any feedback you can give.
Thanks so much for your time!
-Amanda