Hello,
we have a TPS23751 circuit, which is the same as the reference model exept for the feedback circuit. our circuit is designed for 3,8V.
our problem now is that the IC stops gate operation when the input voltage rises above 15V, which makes it unusable for both PoE and aux power input(24V).
i hope someone can help me with this problem, because at this moment we have no idea where this shutdown comes from.
Thanks!