Hi
Looking at the calibration setup;
I have managed to calibrate the voltages successfully.
But when it comes to the temperature calibration, I get an error which suggests that external sensor 3 is out of range.
Our arrangement does not utilise sensor 3 as we are only using a 2S configuration. I haven’t been able to disable sensors 3 or 4 ; or set their offsets to bring them in range?
As it stands I am unable to calibrate the temperature.
I note also that some documents I read allow you to calibrate the sensors individually i.e. internal temperature sensor; ext temperature sensor (thermistor) 1, 2 , 3 and 4. While version 1.3.52 of the BQ studio software only allows one value to be calibrated.
Any help appreciated…
I am also looking to limit the charge current to a standard charge approx.. 1300mA; currently the charge rate hits 2000mA.
thanks in advance for your help