This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

What if any operational impact may result if the UCD9222 PMBUS_ALERT is left floating (without an external pullup)

Other Parts Discussed in Thread: UCD9222

If the UCD9222 is used without any other devices in parallel on the PMBUS_ALERT line, can the line be left floating without an external pullup resistor?

What if any operational impact may result if the UCD9222 PMBUS_ALERT is left floating?

If there is a possible operational impact, is there a way to configure the device so that the PMBUS_ALERT can be left with No Connection and No external pullup?