Hi all,
I have using linux kernel version 4.4.9 . Which driver used for BQ25898 chip ? Below driver can be integrate with our linux kernel ?
Thanks
Tejas patil
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi all,
I have using linux kernel version 4.4.9 . Which driver used for BQ25898 chip ? Below driver can be integrate with our linux kernel ?
Thanks
Tejas patil
Hi,
I was integrate the dirver but compile time it gives error. which kernel source you will integrate ? my kernel verison is 4.4.9
rivers/power/bq25898_charger.c: In function 'bq2589x_psy_register':
drivers/power/bq25898_charger.c:1008:9: error: 'struct power_supply' has no member named 'name'
bq->usb.name = "bq2589x-usb";
^
drivers/power/bq25898_charger.c:1009:9: error: 'struct power_supply' has no member named 'type'
bq->usb.type = POWER_SUPPLY_TYPE_USB;
^
drivers/power/bq25898_charger.c:1010:9: error: 'struct power_supply' has no member named 'properties'
bq->usb.properties = bq2589x_charger_props;
^
drivers/power/bq25898_charger.c:1011:9: error: 'struct power_supply' has no member named 'num_properties'
bq->usb.num_properties = ARRAY_SIZE(bq2589x_charger_props);
^
drivers/power/bq25898_charger.c:1012:9: error: 'struct power_supply' has no member named 'get_property'
bq->usb.get_property = bq2589x_usb_get_property;
^
drivers/power/bq25898_charger.c:1013:9: error: 'struct power_supply' has no member named 'external_power_changed'
bq->usb.external_power_changed = NULL;
^
drivers/power/bq25898_charger.c:1015:39: warning: passing argument 2 of 'power_supply_register' from incompatible pointer type [-Wincompatible-pointer-types]
ret = power_supply_register(bq->dev, &bq->usb);
^
In file included from drivers/power/bq25898_charger.c:20:0:
include/linux/power_supply.h:326:1: note: expected 'const struct power_supply_desc *' but argument is of type 'struct power_supply *'
power_supply_register(struct device *parent,
^
drivers/power/bq25898_charger.c:1015:8: error: too few arguments to function 'power_supply_register'
ret = power_supply_register(bq->dev, &bq->usb);
^
In file included from drivers/power/bq25898_charger.c:20:0:
include/linux/power_supply.h:326:1: note: declared here
power_supply_register(struct device *parent,
^
drivers/power/bq25898_charger.c:1021:10: error: 'struct power_supply' has no member named 'name'
bq->wall.name = "bq2589x-Wall";
^
drivers/power/bq25898_charger.c:1022:10: error: 'struct power_supply' has no member named 'type'
bq->wall.type = POWER_SUPPLY_TYPE_MAINS;
^
drivers/power/bq25898_charger.c:1023:10: error: 'struct power_supply' has no member named 'properties'
bq->wall.properties = bq2589x_charger_props;
^
drivers/power/bq25898_charger.c:1024:10: error: 'struct power_supply' has no member named 'num_properties'
bq->wall.num_properties = ARRAY_SIZE(bq2589x_charger_props);
^
drivers/power/bq25898_charger.c:1025:10: error: 'struct power_supply' has no member named 'get_property'
bq->wall.get_property = bq2589x_wall_get_property;
^
drivers/power/bq25898_charger.c:1026:10: error: 'struct power_supply' has no member named 'external_power_changed'
bq->wall.external_power_changed = NULL;
^
drivers/power/bq25898_charger.c:1028:39: warning: passing argument 2 of 'power_supply_register' from incompatible pointer type [-Wincompatible-pointer-types]
ret = power_supply_register(bq->dev, &bq->wall);
^
In file included from drivers/power/bq25898_charger.c:20:0:
include/linux/power_supply.h:326:1: note: expected 'const struct power_supply_desc *' but argument is of type 'struct power_supply *'
power_supply_register(struct device *parent,
^
drivers/power/bq25898_charger.c:1028:8: error: too few arguments to function 'power_supply_register'
ret = power_supply_register(bq->dev, &bq->wall);
^
In file included from drivers/power/bq25898_charger.c:20:0:
include/linux/power_supply.h:326:1: note: declared here
power_supply_register(struct device *parent,
^
In file included from include/linux/thread_info.h:11:0,
from include/asm-generic/current.h:4,
from arch/arm64/include/generated/asm/current.h:1,
from include/linux/mutex.h:13,
from include/linux/kernfs.h:13,
from include/linux/sysfs.h:15,
from include/linux/kobject.h:21,
from include/linux/of.h:21,
from include/asm-generic/gpio.h:7,
from include/linux/gpio.h:51,
from drivers/power/bq25898_charger.c:15:
drivers/power/bq25898_charger.c: At top level:
include/linux/bug.h:33:45: error: negative width in bit-field '<anonymous>'
#define BUILD_BUG_ON_ZERO(e) (sizeof(struct { int:-!!(e); }))
^
include/linux/kernel.h:831:3: note: in expansion of macro 'BUILD_BUG_ON_ZERO'
BUILD_BUG_ON_ZERO((perms) & 2) + \
^
include/linux/sysfs.h:102:12: note: in expansion of macro 'VERIFY_OCTAL_PERMISSIONS'
.mode = VERIFY_OCTAL_PERMISSIONS(_mode) }, \
^
include/linux/device.h:571:45: note: in expansion of macro '__ATTR'
struct device_attribute dev_attr_##_name = __ATTR(_name, _mode, _show, _store)
^
drivers/power/bq25898_charger.c:1149:8: note: in expansion of macro 'DEVICE_ATTR'
static DEVICE_ATTR(adjvolt, S_IWUGO, NULL, bq2589x_adjust_adapter_volt);
^
drivers/power/bq25898_charger.c: In function 'bq2589x_read_batt_rsoc':
drivers/power/bq25898_charger.c:1222:15: error: 'struct power_supply' has no member named 'get_property'
bq->batt_psy->get_property(bq->batt_psy,POWER_SUPPLY_PROP_CAPACITY,&ret);
^
make[2]: *** [drivers/power/bq25898_charger.o] Error 1
make[2]: *** Waiting for unfinished jobs....
drivers/power/avs/qcom-cpr.c:822:12: warning: 'cpr_disable' defined but not used [-Wunused-function]
static int cpr_disable(struct cpr_drv *drv)
^
drivers/power/avs/qcom-cpr.c: In function 'cpr_probe':
drivers/power/avs/qcom-cpr.c:1176:33: warning: 'step_size_uv' may be used uninitialized in this function [-Wmaybe-uninitialized]
uV = fdata[i].ref_uV + steps * step_size_uv;
^
drivers/power/avs/qcom-cpr.c:1097:13: note: 'step_size_uv' was declared here
int steps, step_size_uv;
^