Hello,
What is the maximum acceptable Junction Temperature, Junction-to-case Thermal Resistance (Theta -JC) and Junction-to-ambient Thermal Resistance (Theta - JA) of the following devices
1) LMZ31710
2) LMZ31530
3) LMZ31704
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Additionally, refer to the safe operating area (SOA) curves in the Typical Characterization section of the datasheet. Operating below the maximum ambient temperature, as shown in the SOA curves, ensures that the maximum junction temperature of any component inside the module is never exceeded.