Hello.
My customers are considering the use of the LM2842.
There is no description of Light Load Operation (Discontinuous Mode) to LM2842's datasheet.
So, I think that is a problem for use in always Discontinuous Mode's Operation.
Is it possible to use the LM2840 in such cases?
<Customer's Power Supply Specifications>
VIN:30V
VOUT:3.3V
IOUT_MAX:420mA
But it becomes Degree less than 5mA, when the microcomputer of latter stage is in the RESET state.
(The intent of the question is concerned about the time of this state.)
Could you tell me in this things?
Best Regards, Masumi Sekiguchi