We have a fan driver circuit from a customer that doesn't work. I think the design intent was to filter the gained-up (logic level) pwm signal. The pi-filter LC section has a cutoff of 72Khz, so I assume it was to be driven with a 100 or 200 KHz pwm signal. It does not work. The mosfet switches too slowly and it really never turns off completely. I am thinking this circuit could be fixed with some sort of improved gate driver for the mosfet.
We need to retain the high-side position of the switching mosfet because the customer fans have "locked rotor" detection circuits that require the fan to be ground referenced. Just replacing the circuit with a buck convertor was considered, but the customer board has separate drivers for 5 different fans, and so the driver circuit needs to be cheap, simple, and small.
I am looking at the tps2819 gate driver, but I'm not sure it will work in this circuit. Having to operate from 24V supply limits available options. Anyone know of a creative way to use this gate driver chip (or some other TI driver) ??