Hi,
A customer of ours is reporting less than desired switching frequency performance. What is the internal capacitance on the RT/CT pin of the UCC28C45? Is it upwards of 50pF? if so, is there a need to compensate for this internal capacitance when setting the oscillator frequency? Also, I am not referring the external timing capacitance that is coupled with the timing resistor on the Vref pin that is used set the oscillator frequency and duty cycle.