This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq78350-R1 Charge Disable

Other Parts Discussed in Thread: BQ78350-R1

The bq78350-R1 TRD, Section 5.5 Charge Disable, lists the safety conditions that can disable charging. This list appears to be incomplete, because the TRD states that the following safety conditions will also set [XCHG] = 1.

CUV Cell Undervoltage Protection

OCD Overcurrent in Discharge Protection

AOLD Overload in Discharge Protection

ACSD Short Circuit in Discharge Protection

OVRD AFE ALERT OVRD Protection

OTD Overtemperature in Discharge Protection

UTD Undertemperature in Charge Protection

 

Is the table in Section 5.5 incorrect?

5.5      Charge Disable


The device can disable charging if certain safety conditions are detected setting the OperationStatus()[XCHG] = 1.

Status

Condition

Action

Normal

ALL PFStatus() = 0 AND

SafetyStatus()[COV] = 0 AND

SafetyStatus()[OTC] = 0 AND

SafetyStatus()[UTC] = 0 AND

SafetyStatus()[OCC] = 0 AND

SafetyStatus()[CTO] = 0 AND

SafetyStatus()[PTO] = 0 AND

GaugingStatus()[TCA] = 0 if Charging

Configuration[CHGFET] = 1

ChargingVoltage() = Charging Algorithm

ChargingCurrent() = Charging Algorithm

Trip

ANY PFStatus() = 1 OR

SafetyStatus()[COV] = 1 OR

SafetyStatus()[OTC] = 1 OR

SafetyStatus()[UTC] = 1 OR

SafetyStatus()[OCC] = 1 OR

SafetyStatus()[CTO] = 1 OR

SafetyStatus()[PTO] = 1 OR

GaugingStatus()[TCA] = 1 if Charging

Configuration[CHGFET] = 1

ChargingVoltage() = 0

ChargingCurrent() = 0

Thanks for helping!

Sheldon