Hi
My customer uses TPS56528.
They have questions about TPS56528.
Could you answer under the questions?
1. If the Power Good doesn't use, should I open PG terminal?
2. There is a mention "A capacitor (typical 0.47 µF) should be connected to GND" about the capacitor of Vreg5 in datasheet.
Can I connect 1uF capacitor between the VREG5 to GND pin?
If a capacitor is connected between GND-VREG5, what kind of operation does this device do?
Best regards,
Yokota