This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5521 - Is the part capable of true 100% output (LEDs continuously ON) ?

Other Parts Discussed in Thread: LP5521, LP55231Part Number: LP5521

Application: LED Constant current driver

Question type: Device selection assistance

Support topic: /Product/Device selection assistance/

Description of the problem: We have 6 independent LEDs (they are not even RGB combination ) in our system to drive (they are single UV-diodes with Ufwd = 4V max.).
We specifically need 100% PWM output = no OFF time, just controll the LED current over I2C.
LP5521 is the only part that we've found and that seems suitable. A lot of other LED drivers seem to offer "constant current LED drive" but after a lot of reading in datasheets one finds out, that they are incapable of true 100% PWM (many go up to 99.6% for example...).
So is LP5521 the right part to use for 100% PWM and setting of the continuous LED current through I2C ?
Is there even a better part ? For example with more outputs (since we have 6 Diodes)?

Thank you,
Zbynek