Hi
Im measuring sw pins waveform
I pulled up sda scl but never sent any i2c command so it should be the same as standalone mode and OTG pin is pulled down
Vbus is 12v
So im expecting
Datasheets figure 55.
But its peak is like 5V
So it loooks more like
Figure 57
And measured current is 300mA from vbus
Im confused
How could i force the ic put in charger mode only ? Let me know
Thank you!