This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq27421-G1D Design energy



Should we set Design energy with default parameter setting?
It is described in quick start guide "When updating the fuel gauge with an EVM using GaugeStudio, Design Energy is automatically calculated based on the type of gauge connected and the Design Capacity." Does this mean design energy is updated automatically after Design capacity setting?
If it is yes, I think it is not needed to set Design energy.

And Load Mode is 1 and Load select is 1 when gauge is default setting. In this case, is Design energy value used for fuel gauge function?
If it is not used, isn't Design energy setting needed?

Best Regards,
Kohei Sasaki