Hello, The TPS61026DRC datasheet specifically calls out the use of a tantalum output capacitor. (Datasheet 11.2.2.3) It also specifically states that the device is not designed for use with ceramics capacitors exclusively in the output circuit. our purchasing wishing to eliminate all tantalum capacitors in our current product design.Currently we are using a 47uf Tantalum mfg pn TPSB476K006R0250 in the C3 designation of the TPS61026DRC datasheet typical application Figure 13. We wish to substitute a MLCC for C3 without changing the circuit or adding a series resistor with the C3 component. Question is: What kind of MLCC can I use to replace the Tantalum without adding a series resistor ( in series with the ceramic) into the circuit or is this not possible or advisable?