This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940L stops working after shorted output

Other Parts Discussed in Thread: TPS25940

I am using a TPS25940 EFuse to protect 8 high-side MOSFET power switches in a 12V system.  I also have a diode in series with the 12V input to the EFuse for polarity protection.  The EFuse is meant to protect against an overcurrent condition, above 3A, or a shorted output, like a wiring mistake.  If I test the EFuse by shorting the MOSFET output to ground, the EFuse shuts down but, sometimes it fails to recover after a power cycle.  From then on, the EFuse will not work.

I checked the EN/UVLO pin and it is at 1.11V and the OVP pin is at 0V (ground).  However, the DVDT pin is at 0V.  If I jump the DVDT pin to the 12V input, the output of the TPS25940 comes-up.

Any ideas why this is happening?  This has happened to 4 or 5 EFuses now.