We have a mature product using the BQ77PL900 in stand-alone mode with an 8S1P cell stack. Our customer returned a unit that fails to charge after 15 months in the field. We probe on the PCBA and find Vpack, Vbat, and all the grounds are connected, but there is no output on Vreg1 (5V) or Vreg2 (3.3V) and the I2C port is not running. Vpack is 24V to there's plenty of margin above Vstartup and the cells are well balanced and all above the UV threshold plus hysteresis. OV is set at 4.25V so no problem there. We use the Vreg2 (3.3V) at VLOG to drive a digital input pin, but there is no other load on Vreg1 or Vreg2. So the Vreg current as <<3mA and the step-down charge pump should not be needed, and indeed it does not seem to be running. We measured capacitance to ground at the Vreg1 and Vreg2 pins so the Verg pins are not shorted. The part appears to be stuck in Shutdown Mode or UVLO Mode even though there's 24V at PACK. So now my questions:
1) Have you seen something like this occur before?
2) Could an over-voltage or ESD-like event happen at the PACK pin 47 that would cause the Vregs to fail?
3) Would the Vregs fail to come up if the bypass capacitors were less than the recommended 2.2uF?
3) Since we can't confirm the register values through I2C, is it possible the register values got corrupted and conflicted the part?
4) Can you suggest how we can proceed to identify root cause for this failure?
5) If the charge pump was running, what waveform would we expect to see at the charge pump pins?