I tested bq27426EVM with bqStudio.
I changed design capacity value to 1000mAh from 1340mAh. However it was initialized to 1340mAh by POR.
How can I change the design capacity value and other parameter?
Best Regards,
Kohei Sasaki
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I tested bq27426EVM with bqStudio.
I changed design capacity value to 1000mAh from 1340mAh. However it was initialized to 1340mAh by POR.
How can I change the design capacity value and other parameter?
Best Regards,
Kohei Sasaki
Hi Kohei,
As you said, your gauge has been initialized by POR.
To solve this ,you could do as below procedure:
1. At your first set-up of gauge, set your parameters in "Data Memory--Gas Gauging-- State--Design Capacity". Then export the Data Memory file(gg.csv) and save it.
2. When your gauge go to POR, just import the file that you save before. Then you can see the parameters will become the value that you set before.
For other parameters, you could do like this, too.
Best regards,
Sammi Shang
Hi Kohei,
If you need re-set some parameters. like capacity, taper current,etc, I think it is better for you to export data memory. You don not need to decide which parameter to be saved, as when you export your data memory, all parameters will be exported.
For some gauges that you mentioned, like bq20zxx, bq40zxx and bq275xx, are all flash-based gauge; but bq274xx is ROM-based gauge. You can judge from the datasheet. Thank you.
Best regards,
Sammi