Hi, I am using a solar panel (SLMD121H10L) that has V_oc = 6.3V, V_mpp = 5.01V, and P_max = 223mW and one Lithium Polymer battery . I'm looking for a PMIC that has the same features as bq25570 ( it has over/under voltage threshold protecting battery from overcharge and over-discharge, MPPT, etc.) The only problem for bq25570 is its V_in range from 0.1~5.1V which lower than V_oc from the solar panel. I have hard time finding an alternative PMIC that fits the PMIC and the battery. Is there any advice? Thanks in advance.