Hi,
we use gauge IC BQ27542-G1 to monitor the battery status. The communication protocol is HDQ.
A abnormal current value is always read. when the device is charging , the value of reg 0x14 is 0x210(528mA), and is 0x1C6(454mA) when discharging.
Normally, the current value should be a negative number.