This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LMR64010 using instead of LT1930

Other Parts Discussed in Thread: LMR64010

 Hi guys,

 One of our customer wants to use LMR64010 instead of LT1930 because the both devices are pin compatible. The customer is using the application circuit, "±15V Dual Output Converter with Output Disconnect" showed on page 8 in LT1930 datasheet (http://cds.linear.com/docs/en/datasheet/1930f.pdf) .

 Is it no problem to use LMR64010 for the application circuit?

 Your reply would be appreciated.

 Best regards,

 Kazuya Nakai.