Hi all
Would you mind if we ask BQ24250?
The datasheet on P8 shows about STAT/INT pins as follows;
"When a fault occurs, a 256μs pulse is sent out as an interrupt for the host."
<Question1>
What does "a fault occurs" indicate?
<Question2>
Does "a fault occurs" mean the same as "FAULT CONDITION" on the datasheet P30?
<Question3>
And then, in relation to <Question2>, does TS Fault indicate b0 to b2 of Register #6?
Except 000(b0 to b2)(No TS fault), TS fault occurs, and then STAT pin is sent out with a 256μs pulse, right?
Kind regards,
Hirotaka Matsumoto