I want to use BQ24157 in large current mode, referred to the datasheet, I should connect the OTG pin to high level.
Should I connect to the input of USB(VBUS), or to the Battery side?
My friend connect it to the output of a LDO, and the LDO connect to the output of BQ24157. Is it OK?
Thank you!