This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Is the GPIO3 pin processing of TPS65218 correct?

Other Parts Discussed in Thread: TPS65218

Hi,

There is a question about GPIO3 pin processing of PMIC(TPS65218).
There is the following description to the data sheet of TPS65218.
7.3.1.14 I/O Configuration
GPIO3:
General-purpose, open-drain output controlled by GPO3 user bit or sequencer
Reset input-signal for DCDC1 and DCDC2

DC12_RST bit of CONFIG2 Register is set to 1 in RESET and is chosen as follows.
GPIO3 is configured as warm-reset input to DCDC1 and DCDC2

With following document and AM437x EVM and AM437x SK board, it becomes the open processing.
Figure 2. Connection Diagram for TPS65218 and AM437x
www.tij.co.jp/.../slvuaa9.pdf

Our customer doesn't use warm reset.

It is thought that it becomes the low recognition when a noise occurs when it is open processing, and reset may occur.
Should the processing of right pins make pulling up?

Or it is open-drain output, and does GPIO3 not have any problem by pin processing of open after sequencer start because it is described to a data sheet with "General-purpose, open-drain output controlled by user bit or sequencer"?

Best Regards,
Shigehiro Tsuda