I am using BQ24773 in a circuit that has:
-Micro USB port for charging, driven by a benchtop linear supply capable of supporting 2A (current limit at 2.1A) at 5.05V DC
- Battery pack, using 4 x 18650, Panasonic cells, NCRE18650BE, which are configured 1S 4P, with our safety circuit including PTC fuse and SMTl fuse (non resettable) and independently monitor an I2C temperature sensor on the battery.
So this is a 3.2A x 4 = 12.8A total capacity, of which 8A is usuable running to 3.2V.
When the system is in hibernation, the total current draw is 50nA from the Vsys port.
The charge time is excruciatingly long - ~30 hours for full charge.
The system is set to have the WDT disabled, 2A charge current, 3.2V minimum. Monitoring the charge control registers, it seems to be working normally.
I should mentioned the circuit is nearly identical to the evaluation module - in component choice and layout. The only variation is I am using a 3.3uH inductor instead of the 2.2uH inducator due to part availability.
Why is the charge time so long? How do I improve this? I would expect to see a full charge, which I designate as 3.2V when 'fully depleted' to 4.2V 'fully charged' - 8 A/h, tobe approximately 5 - 6 hours with loss?
30 hours is not acceptable.