Hello,
Could you help to advice for suited PMIC part number for freescale processor of the MCIMX6U5EVM10AC?
Thanks, Regards,
Brian
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
Thank you for reaching out to us. Please consider the TPS659114 device.
Product folder is located here: 
We have an application note for the I.MX6 Dual and Quad implementation of this device located here:
.
Please let us know if you have any questions!
Thanks for your suggestion.
There is another inquiry of PMIC for HMI application. Delta HMI team is looking for the PMIC for the MCU chip: RockChip RK3288
Current soluiton for RK3288 is RK818/808. I am not sure if any TI PMIC can replace it? Very thanks.
Regards,
Brian
Hi Brian,
Please consider TPS65086. I need to ask some additional questions so I will follow up with you offline.
Hi Brian,
We do not have any integrated buck solutions that are currently configured for the processor. We do have a device coming out which was configured from the TPS65910, but the device doesn't meet the max currents on the VDD_ARM_IN rail. If the customer only plans to run typ range on that rail, you may consider TPS65910 as an option.