Hi TI Experts:
I have a customer that would like to use Buck DCDC, TPS62770.
It have 1 stepdown and 1 stepup output.
The Buck DCDC do have an extreme low Iq but they only need the stepdown output.
According to the datasheet, the stepup DcDC will turn off if the Enable pin is in low condition.
But it did not mention the current consumption of the DCDC if it’s the Stepup DCDC is in off stage.
If the stepup portion is disable, did it still draw current?
Please advice,
Thanks,
Br,
Teach me