This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z100 EVM

Other Parts Discussed in Thread: BQ34Z100, BQSTUDIO

Hi,

I am testing the BQ34z100 evm with a 4S battery. I configured the evm using jumpers to achieve the following:

-jumper to allow more than 1 LED (J1)

-16V (J2)

-Alert configuration with A (J3)

-Multi-cell mode (J5)

-4 internal LEDs (J6)

-I2C communication (J7)

I faced the following problems:

1)  I was  not able to establish a communication between EV2300 and the BQ evaluation software. I connected the I2C port of the BQ34z100evm to that of EV2300.

It showed a "No Acknowledge: VB_T2H_NACK" message.

and

I measured the voltage on Q3.

Q3 Gate        5.5V

Q3 Source   3.5V

and REG25  0.06V

What should I do next.

Thanks!