Hi team,
My customer is evaluating BQ24190 now. They have no idea how to set the charging current. the charging current is only 120mA on the BQ24190EVM-021.
Enviroment setup:
1. Bq24190EVM-021 :CE PIN connect to GND (JP5), Jump PULLUP (JP3)
2.input VBUS has the power supply
3. the output load BAT connect either to battery (H103450 1850mA) or Keithley 2302 single channel battery simulater.
4. customer tried to tune the R15 resistor. The charging current is still the same.
Can you provide your suggestion how to tune the charging current?
Thanks,
SHH