Hello
Is it possible to use TPS54531 in negative configuration, to get -12V from +15V input?
I'd use another TPS54531 in parallel to get +12V from the same +15V.
If I didn't explain well, I'd like to use TPS54531 with this approach:
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Thank you.
By looking at those app.notes, it seems that I can't simply "reverse" GND and positive output, instead I should also change the components values and not keep those suggested by the Webench for the positive application, is that right?
I would probably use whatever the calculator tool provides. It was designed specifically for inverting buck boost topology. In the past I have used webench for 27 V input to 12 V output to get "close".
I would use the calculator tool, but TPS54531 isn't listed in the deveice selection menu.
I'm not familiar with the others devices supported, which other one could I use to approximate the calculations? maybe TPS54331?
That is somewhat surprising. I did not personally develop that tool, but I would expect the compensation to change with the varying power stage parameters. I tried a coupe different ICs and notice that you are correct. Very little changes. Let me see if I can track down the author of that tool and find out what is going on.