This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Reference design for H-bridge Non-isolated inverters

Other Parts Discussed in Thread: UCC28950, UCC27714, UCC27210

Hi team,

I was wondering if there is a reference design available for H-bridge Non-isolated inverters. Could you please point me to the app note or the document?

Thanks & Best Regards,

Rohit

  • Hi Rohit,

    What BUS voltage do you intend to run the H bridge from ?

    We have the UCC27714 which is a 600V rate 1/2 bridge driver. There is an EVM available and it used the UCC28950 phase shifted full bridge controller with two UCC27714 drivers to provide the gate drive voltage to the H Bridge mosfets.

    The HPDS product line also has a number of 100V and 200V 1/2 bridge drivers for use in lower voltage applications, such as LM5100, UCC27210,

    Regards

    Peter