The TRM of bq78350-R1 mentions the use of Chem ID to estimate Initial Battery Capacity at Device Reset.
Is Chem ID also used in CEDV / Impedance track features of the host ? If so which are the parameters/registers affected with a change in Chem ID ?
Does the Host use Max Cell voltage or Min Cell Voltage or the ExtAvgCell Voltage for estimating the RemCap ?
Currently using Chemistry database Version 528
and host FW v1.03 build 22