I am experimenting with a 24298EVM board. I am using this in standalone mode.
I have a load connected to the SYS output (3ohms).
PSEL is pulled low via JP1.
R19 is turned completely counterclockwise so that ILIM is set to max (3A).
If I have a charged battery connected to the IC, the system will start up normally when I plug the adapter in (PG goes low, and the SYS output goes to 4.15V). The appropriate current draw from the adapter occurs (~1.7A).
If I remove the battery and then plug in the adapter, PG stays unlit and SYS output does not go active. There is a 100mA draw on the adapter. It does not start up properly,
If I remove the load from SYS, it will start up properly when I plug in the adapter. I can then connect the load and everything works OK.
Why won't it start up without a battery? Yes, it will normally have a battery in it, but why is it required? Even if it were installed, it might be completely drained and disconnected from the circuit via its PCM - this is the state it will be in if the battery dies and the user lugs it back in.