Hi there,
I am trying to design a fully controlled bidirectional 3ph AC to DC unit connected to power grid in US. I am using 3 of UCC27714 as the driver to drive 6 IGBTs (IXGN200N60B3). I have an issue with the higher switch Gate signal. When I send the control signal from the uC to driver to turn on the IGBT, the driver should raise the Gate voltage about 15 volts higher than Emitter so the IGBT turn on (boot strap). But it wont. As an experiment I connected the Emitter of the higher IGBT to DC GND and the driver started to work. To me, it looks like that Emitter in the middle needs a reference voltage or something.
I do not have this issue when coming from DC to AC. Means if I connect the DC source and try to turn on the IGBT that is fine, but it does not fire reversed.
I appreciate your ideas.
BTW in the schematic you see a Mosfet with diode and snubber circuit but on the actual board I have only IGBTS with no diodes no snubbers. 6 switch bridge and a driver circuit is attached.
Best
Ashkan