Hello,
TPS62160 appears to have switching jitter at low input voltage and high duty cycle. The below conditions and measurements were made on the TPS62160EVM. Output voltage was set to 3.3V. This same behavior was also seen on prototype boards.
4.20V - 4.36V @ 200mA
4.33V - 4.50V @ 400mA
4.59V - 4.74V @ 800mA
Can you comment if this is normal behavior, and if so, is there a way to avoid it by adjusting the external component values?
Thanks!
Keith N.
AFA OH/wPA