This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5122-Q1 PMP7950 and PMP9309 circuit



PMP7950 and PMP9309 circuit has parallel low side FETs. Is this because you are taking into account the heat generation?

How did you decide inductor value? I think this circuit's ripple current is large.

Our customer requirement is the following,
Vin: 9V to 45V (Typ: 28.5V)
Vout: 85V
Iout: 2A

Do you have reference circuit for above requirement? If you have any idea, please let me know.
Is it possible to achieve by reducing sense resistor value of PMP7950 circuit?

Best Regards,
Kohei Sasaki