This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ78350-R1, Setup for High capacity

Other Parts Discussed in Thread: BQ34Z100, BQ78350-R1

Dear sir.

We have a difficult setup for high capacity.

Voltage : 12.6V (3S16P)

Capacity : 41.6A

Battery : SAMSUNG INR18650-26F

Scaling : 2x divide

-------------------------------------------------

Currnently voltage : 11.6V

SOC : 30%

-> Something is strange.

------------------------------------------------

1. We want to know how to fix(setup,modify) any part  in the program by picture.

2. if the capacity is 41.6A, divide into 2, Is right?

3. The manual(bq34z100) is not understand.  We used the bq78350-r1.

    So, Tell us in the picture. please.....

Thank you and best regards

  • Hi, I apologize that no one has followed up with your question posted last year due to the large number of questions we got towards the end of 2016, please feel free to post a brand new question should you still need an answer instead of replying to this post. We will do our very best to respond in a timely manner to any new post you might have :-)
    Best Regards,
    Haidar