Hi All,
I am unfamiliar with our Power Modules and wanted to ask a question with relation to the no load current.
If the PTH12050W is supplied with 5V and there are no caps input or output, would the 'Input standby current' go from drawing 10mA, to approx. 100mA?
I am keen to help my customer get to the bottom of the overheating of part (approx. 80 degrees C) when under a no load condition. My customer has so far connected a PSU voltage of 5V to the module.
Many thanks,
Ross