Our customer is using LM5116 with VCCX pin Open.
VIN:32V
VOUT:5V
VCCX:Open
Please let us know what kind of bad thing happen when they open VCCX.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Kura,
We don't recommend that the VCCX pin be left open, if not used it should be grounded.
If it is left open and there is a capacitor on the VCCX pin, there should not be any catastrophic failures.
If it is left open with no capacitor, you may have noise coupled into the controller and there maybe erratic controller behavior.
Terry
Kura,
Are you asking if there is a capaciot on the VCCX pin, what would cause it to fail? If so I would think an over voltage.
Terry